Regeneration - Raise Rods
When the load lifts, energy goes into motor from the drive, then into the machine from the motor. When this happens, the motor and rotation are in the same direction, meaning the system is operating in a “motoring” or "consumption" mode.
Lower Rods» Raise Rods»