Step 1:
Add A Module

Add a new module using an add-on profile

Step 2:
Configuration

Configuring a new ArmorStart module using the add-on profile

Step 3:
Going Online

Download and go Online with a new module

Step 4:
Status and Diagnostics

Provides an abundance of useful information

Step 5:
Configuration Tags

Using Configuration Tags

The embedded webpage provides the users a lot of flexibility to determine the status and diagnostics of the ArmorStart LT. The webpage can also be used to configure many of the networking parameters or the email functionality. The following is a self directed interactive example of the webpage used with EtherNet/IP enabled ArmorStart. Notice the extensive and product and network diagnostic information that is this available with the webpage which is presented in real-time.